nl(l
SUJITCH
D. lSJSS
Series FF01 Emergency Stop Switches
www.nkkswitches.com
8
Installation of Switch
Safety Precautions
• Read the FF01 Series Instruction Manual before switch installation, cable connection, operation, maintenance or inspection.
• Confirm power is off before installation, cable connection, maintenance, etc.
• When installing product on other equipment, be sure usage is in compliance with standards and regulations of your country
or region, as required for your system, equipment or facility.
• Use the switch at the voltage and current recommendations in the specifications. Exceeding these may cause overheating.
• Use wiring with the appropriate rating.
• Follow recommended panel cutout dimensions and mounting instructions or switch may not operate properly.
• Remove dirt and dust from switch mounting surface of the panel before beginning installation.
• Do not disassemble the product, as it may cause malfunction, electric shock or fire.
• Operate switch by hand only; do not operate using foot, tool or other object.
• Bouncing may occur during a reset operation (pull or turn to reset). If switch-mounted equipment is subjected to shock or
vibration, it may cause chattering. Take appropriate measures to prevent bouncing and chattering on the equipment side.
• Do not drop the switch or apply excessive shock or vibration. Deformation or damage may cause malfunction or performance
degradation.
• After inserting the lead wire into the terminal hole, use a soldering iron to ensure a secure connection.
• If soldering is executed with terminals facing up, avoid allowing the flux to enter the interior of the switch.
• Soldering temperature is 390°C maximum within four seconds.
Usage Environment
• This product is designed for indoor use.
• Avoid using the switch in environments where there is frequent splashing water.
• If the switch becomes wet, wipe off with a dry cloth. Using a switch exposed to water may result in water entering inside. If
the water freezes inside the switch, it may not function properly.
• In an environment where dust and dirt may accumulate, remove deposits
around switch before use. When necessary, a cloth dampened with a
small amount of neutral detergent may be used. Follow using a dry cloth.
Installation of Switch into Panel
1. Remove the nut from the switch body.
2. Insert the switch body into the panel, aligning notch on the o-ring with
the anti-rotation tab on the switch body. Align the anti-rotation tab on
the switch body with the anti-rotation keyway on the panel.
3. Using the AT119 Socket Wrench, tighten the nut from back of panel
(recommended torque 785mN•m).
SAFETY PRECAUTIONS & INSTALLATION INSTRUCTIONS
Anti-rotation Tab
on Switch Body
Notches
on O-ring
Anti-rotation
Keyway
on Panel
7850 East Gelding Drive • Scottsdale, AZ 85260 • Telephone 480.991.0942 • Fax 480.998.1435
www.nkkswitches.com • 1.877.2BUYNKK (228.9655)
Effective Date May 2020