Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Change Card

Now that all of the code required has been ported to the OTP device, the hardware can be set up to allow the user to program and test the application. Replace the daughter board with the C8051F34A device for the daughter board with the C8051T62x socket adapter. Plug the daughter board onto the P1 and P2 connectors of the mother board. Place one of the sample devices in the socket adapter making sure the pin one designations line up.

PTM Published on: 2011-06-02