Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Analog 2

On the C8051F34A, the ADC can use one of three different voltage reference options: the VDD supply pin, an external reference applied to the VREF pin, or the on-chip 2.4 V reference voltage routed to the VREF pin. In the C8051T620/T320/T321 family, two additional voltage reference options are available. By setting the REGOVR bit in the REF0CN register, the ADC can use the internal regulator as the voltage reference for the ADC. If using the on-chip reference voltage generator, the REFBGS bit can also be used to switch between 1.2 V and 2.4 V. Use of the temperature sensor is very similar to that of the C8051F34A. However, the transfer functions of the temperature sensors on each device family are different. Different values for the offset and slope of the temperature sensor are necessary to accurately calculate the temperature on each device family. Additionally, to help remove some of the error due to part-to-part variations, the temperature sensor output has been measured during production test for each device and stored in EPROM. The value represents the output of the temperature sensor at an ambient temperature of 0°C, if measured with the ADC using the internal regulator as a reference voltage.

PTM Published on: 2011-06-02