In summary, as the world demands faster and higher performance in every application, new memory technology is needed to enable smarter solutions. FRAM from Texas Instruments provides unified memory with dynamic partitioning and memory access speeds 100 times faster than flash. FRAM is also capable of zero power state retention in all power modes, which means that writes are guaranteed, even in the event of a power loss. Additionally, with a write endurance of over 100 trillion cycles, EEPROM is no longer required. All of this is possible at less than 100 μA/MHz active power consumption – a first for the semiconductor industry.