Webinar – Seven Reasons to Move from 12 V to 48 V Today
A discussion on why 48 V is becoming the dominant power delivery network and how modular power solutions can speed and simplify transition.
Simplifying Frequency Stability for High-Speed 5G and Data Converter Designs
Publicatiedatum: 2026-03-25
Discover how ADI's ADF4382 PLLs with integrated VCOs enhance frequency stability and speed for high-speed data converter and 5G radio designs.
Building Quantum-Resilient Embedded Systems with iWave’s Agilex™ 5 System on Module
iWave Global has partnered with Xiphera to deliver quantum-safe cryptographic capability on iWave’s Agilex™ 5 System on Module (SoM) powered by Altera.
How to Select Cables for Reliable VFD Motor Control and Sensor Feedback
Publicatiedatum: 2026-03-24
Growing industrial automation and the push for better energy efficiency are speeding up the adoption of VFDs in motor-driven systems.
Solder Smarter Using DigiKey Standard Helping Hands
Explore DigiKey Helping Hands features including magnetic PCB pillars, flexible arms, LED magnifier, and a heavy steel base for stable soldering.
Automotive Ethernet: The Backbone of Modern In-Vehicle Communication
As vehicles become more autonomous and data-centric, the need for a high-speed, scalable, and reliable in-vehicle communication backbone is greater than ever.
Webinar – Select the Right Cables for Harsh Industrial Automation Applications
This in-depth webinar breaks down what it takes to select the right wire and cable for industrial environments.
Pushing the Limits: A 6km LoRa Range Test with the PTSolns SX1276 Shield
In this blog, we’ll explore the hardware that’s being used, the science behind the transmission, and just how impressive a feat it is to achieve a 6km range.
How Hardware Gets Hacked (Part 2): On-boarding
Explore a hardware security workflow using firmware builds, simulation tools, serial commands, and automated tests for microcontroller systems.
Detecting High-Impedance Ground Faults: Limitations of Standard GFDI and Active Diagnostic Solutions
Publicatiedatum: 2026-03-18
An examination of the limitations of standard GFDI, the physics of high-impedance faults, and the practical challenges of locating them in 1500 V arrays.
Criteria for Cable and Wire Selection
Publicatiedatum: 2026-03-17
Cable design needs to focus on the system concept, integrating the installation method, electrical and mechanical loads, as well as cost-effectiveness.
Why We Need New Op Amps Despite Already Having So Many Good Ones
Older op amps offer designers confidence, while new ones offer vendors the potential for long-term bill-of-materials winners.
How to Overcome Linux Development Hurdles in Resource-Constrained Systems
Publicatiedatum: 2026-03-12
Learn how the BeagleBoard.org BeagleV-Fire single-board computer addresses common hurdles for running Linux in resource-constrained systems.
Webinar – Single Pair Ethernet — Simplified Sensor-to-Cloud Networking
Single Pair Ethernet (SPE) has reshaped industrial connectivity. Now, with Power over Data Line (PoDL), SPE can deliver both data and power.
XRP CoreXY Chessboard Reimagined
Discover how the XRP CoreXY chessboard prototype evolved with improved durability, lighting effects, and a compact transportable design.
How to Meet High-Speed Interface Requirements Using Hyper Cool Edge Connectors
Learn how the Hyper Cool Edge connector family can be used to support high-speed data interfaces for applications such as storage and AI datacenters.
PetaLinux NVMe Break Through 7 GB/s on the AMD ZCU106 Evaluation Kit with Design Gateway’s Solution
Publicatiedatum: 2026-03-11
An introduction to the world’s first NVMe PetaLinux solution operating at PCIe Gen4 speed without relying on the PCIe Hard Block of the FPGA.
Electronics Teardowns and Recycling
A beginner-friendly guide to disassembling electronics, salvaging parts, and disposing of e-waste responsibly.
Simplify AMR and AGV Integration with ROS 2 Components
Publicatiedatum: 2026-03-10
Accelerate AMR and AGV integration using motor controllers, IMUs, and ToF modules with native ROS 2 drivers.
Getting Started with the Microchip VeryVerilog Kit
Follow the setup and programming process for the VeryVerilog kit, including firmware loading and exploring built-in logic demos.