IO-Link: Making the Connection from Sensor to Edge Computing
Bijgedragen door DigiKey
2026-02-12
Every production line in a factory generates vast quantities of sensor data, yet much of that information has historically gone untapped. The reason is that conventional sensor connections rely on basic switching signals or analog outputs that deliver a single process value with no additional context about device health or operating conditions. IO-Link addresses this limitation head-on, providing a standardized digital communication layer (IEC 61131-9) that gives sensors and actuators a direct, bidirectional dialog with the wider control architecture.
Figure 1: Every production line in a factory generates vast quantities of sensor data. (Image source: Adobe Stock)
Rather than replacing existing fieldbus or industrial Ethernet infrastructure, IO-Link operates as a complementary interface at the lowest level of the automation hierarchy, using the unshielded three-wire or five-wire cabling and standard M5, M8, or M12 connectors manufacturers already stock, with cable runs supported up to 20 meters. Each IO-Link device connects to a dedicated port on an IO-Link master, which aggregates field-level data and relays it upward to programmable logic controllers (PLCs), Edge gateways, or Cloud platforms, preserving existing investments and opening up a high-resolution data channel down to the individual sensor.
Turning reactive maintenance into predictive strategy
Most facilities still oscillate between one of two maintenance models, neither of which is ideal. Reactive maintenance essentially waits for failure, often resulting in unplanned downtime and rushed repairs, while calendar-based preventive schedules can trigger component swaps long before they are actually needed. IO-Link offers a third option by equipping maintenance teams with continuous, sensor-level diagnostics that reveal how equipment is actually performing in real time.
A good use case for IO-Link devices is a pressure sensor on a pneumatic assembly station. With a standard analog connection, it reports only the current pressure value. However, an IO-Link-enabled version of the exact same sensor can simultaneously communicate internal temperature, cumulative operating hours, signal strength, and any fault codes, all over the same three-wire cable. Similarly, a photoelectric sensor monitoring parts on a conveyor can flag progressive lens contamination long before its detection accuracy deteriorates to the point of missed readings. These granular diagnostics allow teams to determine maintenance intervals based on actual device conditions rather than assumptions, avoiding premature replacements as well as unexpected breakdowns.
When a sensor does eventually require swapping, the IO-Link’s built-in data storage function accelerates the process significantly, since the IO-Link master retains the previous device’s full parameter set and writes it automatically to the replacement unit within seconds. Consequently, technicians can complete a swap without manually re-entering settings, lowering the mean time to repair and keeping production lines moving with minimal interruption.
Improving quality assurance through digital transparency
Reliable quality assurance is based on measurement consistency, and that is precisely where analog sensor connections introduce risk. Analog signals degrade over long cable runs and are vulnerable to electromagnetic interference, meaning the value a PLC receives may differ subtly from what the sensor actually measured. While this seems like a minor risk, across hundreds of measurement points in complex production environments, these small inaccuracies accumulate and can push processes outside acceptable tolerances. Again, IO-Link removes this variable by converting measurement data into a digital signal at the sensor itself, ensuring that the reading arriving at the controller exactly matches the value captured at the source.
IO-Link can also improve how facilities handle product changeovers. In filling lines, packaging systems, and multi-variant assembly cells, switching between product recipes typically requires technicians to adjust sensor parameters manually, a process that is time-consuming and prone to configuration errors that can trigger quality deviations on the first batches after a changeover. With IO-Link, the PLC can push new parameter profiles to connected sensors simultaneously, completing a full recipe change in seconds rather than minutes, and because these profiles are stored digitally and recalled on demand, each changeover is always identical to the last.
Driving productivity from the sensor to the Edge
The bidirectional flow of data IO-Link systems does more than improve sensor performance, as it also creates an end-to-end information pipeline connecting the factory floor to enterprise-level analytics. IO-Link masters can consolidate field-level data and expose it via industrial Ethernet protocols like PROFINET, EtherNet/IP, and EtherCAT, making it accessible to Edge gateways that run local preprocessing and low-latency decision logic. The same data can be forwarded to MES, ERP, or other Cloud-based platforms for broader operational intelligence.
This sensor-to-Edge architecture enables monitoring scenarios that would be impractical using conventional wiring. For example, a compressed air system can be instrumented with IO-Link flow sensors that report consumption data digitally, enabling facilities to pinpoint leaks, track energy costs per machine, and optimize the pneumatic performance without deploying separate monitoring hardware. The same digital backbone supports cooling circuit surveillance, conveyor health tracking, and environmental condition sensing across the entire plant.
The benefits also extend to installation and commissioning, since IO-Link devices are identified and configured automatically through their IO Device Description (IODD) files, making initial setup faster and less dependent on users with specific knowledge. By eliminating analog PLC input cards, manufacturers can streamline system design with per-point wiring cost reductions compared to analog installations. Interoperability across more than 500 device manufacturers worldwide also ensures that facilities can scale without being locked into a vendor’s ecosystem.
DigiKey’s IO-Link solutions: from sensors to systems
Deploying an IO-Link system means selecting the right combination of sensors, masters, and connectivity components from suppliers with genuine depth in industrial automation. DigiKey's IO-Link product catalog brings together the full ecosystem from five leading suppliers, each contributing distinct strengths.
Figure 2: Festo IO-Link devices. (Image source: Festo)
Festo draws on decades of pneumatic and electric automation expertise to deliver an extensive IO-Link lineup of pressure sensors, flow sensors, position transmitters, and valve terminals. Its CPX-AP-I decentralized I/O platform includes a 4-port IO-Link master module with IP65/67 protection for on-machine installations, and its IO-Link-enabled sensors feature software-switchable PNP/NPN outputs and built-in data storage for rapid commissioning and seamless device replacement.
Figure 3: ifm IO-Link solution. (Image source: ifm)
As a founding member of the IO-Link community, ifm has built one of the broadest IO-Link device catalogs available. Its sensor portfolio operates on fully digital signal transmission, sidestepping the accuracy losses that typically plague analog-to-digital conversion in legacy installations. Beyond sensors, ifm's ecosystem extends to Edge gateway devices that securely route field data to Cloud platforms including Microsoft Azure IoT Hub and AWS IoT Core, providing a streamlined path from shop-floor sensors to enterprise-grade analytics.
Figure 4: SICK IO-Link devices. (Image source: SICK)
SICK pushes IO-Link further through its Smart Sensor Solutions and Sensor Integration Gateway (SIG) families, which add embedded intelligence to field-level devices. Its IO-Link sensors can execute decentralized Smart Tasks like counting and length measurement directly on the device, reducing the processing burden on the PLC. SICK’s FieldEcho software complements these sensors by providing browser-based access to all IO-Link device data, handling IODD downloads automatically, and exposing a REST API for integration with MES, ERP, and Cloud services.
Figure 5: Pepperl+Fuchs IO-Link technology. (Image source: Pepperl+Fuchs)
Pepperl+Fuchs contributes deep experience across both factory and process automation, pairing a wide sensor range of inductive, capacitive, photoelectric, and ultrasonic devices with robust master infrastructure. Its ICE11 IO-Link master stands out for its multi-protocol flexibility, supporting PROFINET, EtherNet/IP, EtherCAT, CC-Link, and MODBUS TCP from a single device, while its IIoT starter kit bundles a master, sensors, and all required cabling for rapid prototyping straight out of the box.
Figure 6: iTEMP TMT36 temperature head transmitter with IO-Link. (Image source: Endress+Hauser)
Endress+Hauser brings process instrumentation heritage to DigiKey's IO-Link offering, with particular strength in food and beverage, water treatment, and pharmaceutical applications. IO-Link temperature sensors and pressure transmitters offer a dual-mode capability, operating in either traditional analog (4-20 mA) or digital IO-Link mode through a simple configuration change, letting facilities adopt digital communication incrementally while preserving existing workflows.
Conclusion
IO-Link has quickly evolved from a niche connectivity option into a critical enabler of data-driven manufacturing, with a rapidly expanding global installed base and broad vendor support across multiple industries. By delivering bidirectional digital communication over standard industrial cables, this technology equips manufacturers with the sensor-level visibility needed to predict maintenance issues, maintain measurement precision, and channel real-time field data to Edge and Cloud platforms where it can drive continuous improvement.
Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.