Compliance Trap Snapping Shut on Flame-Retardant Cables

Flat flex cables (FFCs), often overlooked when products function well, can suddenly become a focal point for system review due to changes in compliance standards. Designers now face challenges with a so-called compliance trap, as halogen-free requirements and evolving regulations increasingly constrain the use of Decabromodiphenyl Ethane (DBDPE), a brominated flame retardant commonly used in cables.

DBDPE was widely adopted as a flame-retardant additive primarily utilized in plastics and electronic components to replace Decabromodiphenyl ether (DecaBDE), which was widely restricted in some regions and voluntarily phased out in the U.S. While DBDPE has remained in widespread use, it now sits within a broader category of halogenated flame retardants that is increasingly under regulatory and procurement pressure.

In November 2025, the European Chemicals Agency (ECHA) designated DBDPE as a Substance of Very High Concern (SVHC) under the EU's REACH (Registration, Evaluation, Authorization, and Restriction of Chemicals) chemical safety regulations. Canada and Australia had already begun constraining DBDPE’s use before the EU formally elevated it into its SVHC assessment framework.

The ECHA raised the stakes for designers when it set an abrupt deadline of May 6, 2026, for mandatory disclosures when concentrations exceed 0.1% by weight (weight/weight, or w/w). Considering that such concentrations in FFCs typically range between 2% and 8%, the EU designation raises the threat of future regulatory liability for products that today are technically compliant, hence the compliance trap.

For product designers, DBDPE creates a moving compliance target for a material that is acceptable at design-in but may later require substitution, redesign, or requalification as restrictions tighten across jurisdictions. In addition to immediately updating Bills of Materials to reflect disclosure requirements, product designers would be well advised to speedily adopt FFCs that don't include the chemical.

Environmental credentials at risk

Suppliers are now obligated to provide customers, and potentially consumers, with sufficient information to ensure the safe use of a product that includes DBDPE. Products containing SVHCs like DBDPE are generally disqualified from receiving the EU Ecolabel certification, so even a single non-compliant FFC could compromise the marketing of finished product environmental credentials.

Long after thermal testing is complete, certifications are approved, and production ramps smoothly, a DBDPE presence could trigger redesigns, customer pushback, or compliance reviews across entire product lines. Manufacturers cannot simply dilute a formulation to bring it under the threshold, but will likely push requirements down their supply chains to effectively filter out the use of DBDPE.

Connector and cable assembly solution provider GCT offers a way out of the dilemma with a new line of drop-in halogen- and DBDPE-free FFC cables (Figure 1) in a 0.5 mm pitch with 4 to 80 circuits, and a 1.0 mm pitch with 4 to 50 circuits. According to CTI testing, the FFC jumper insulator samples submitted by the company returned a "not detected" rating for DBDPE.

Figure 1: Rendering of GCT's halogen- and DBDPE-free flat flex cables. (Image source: GCT)

The new GCT FFCs fully address the flame-retardant expectations engineers design around, with a different material system that aligns more closely with current OEM and environmental expectations. Simplifying the transition, the company is mirroring its existing part number configuration with the addition of "-HF" to designate the halogen-free nature of its cables.

These halogen-free constructions are engineered to preserve flex endurance under repeated bending, maintain dimensional stability under thermal cycling, and retain compatibility with existing connector systems. This allows designers to change materials without altering the mechanical or electrical envelope of the product, while meeting requirements for high-density assemblies where space and routing are already fixed.

Finally, and increasingly importantly, these cables are designed with long-term compliance stability in mind. OEMs are no longer waiting for formal bans to act. Halogen-free requirements and restricted-substance policies are effectively compressing the usable design window for brominated systems. In practice, material decisions made today are increasingly judged not only on compliance at launch, but on their ability to avoid redesign, requalification, and supply-chain disruption as global standards continue to converge.

Conclusion

By eliminating DBDPE and other halogenated additives at the cable level, GCT’s approach reduces the risk of downstream redesigns, requalification events, or procurement barriers as regulatory frameworks tighten use of the chemical. Because the cables don't change the electrical or mechanical interface requirements, designers and OEMs can use them to quickly shift away from DBDPE and to prepare retrofitting strategies to address the potential implementation of more restrictive regulations and customer requirements.

Achtergrondinformatie over deze auteur

Image of Pete Bartolik

Pete Bartolik is een freelance schrijver die al meer dan twintig jaar onderzoek doet naar en schrijft over IT- en OT-kwesties en -producten. Daarvoor was hij nieuwsredacteur van de IT-managementpublicatie Computerworld, hoofdredacteur van een maandelijks computertijdschrift voor eindgebruikers en verslaggever bij een dagblad.

More posts by Pete Bartolik
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum