Maker.io main logo

Unlocking the Power of Verilog Operators - Part 10 of our Verilog Series

880

2024-03-08 | By DWARAKAN RAMANATHAN

What are Verilog Operators and its types:

In Verilog, operators are symbols or special characters used to perform various operations on data, such as arithmetic calculations, logical comparisons, and bit manipulation. Verilog operators allow you to manipulate and process signals and data within your hardware description, making them a fundamental part of the language. Verilog operators can be categorized into several types, each serving a specific purpose:

1. Arithmetic Operators:

  • + (Addition): Adds two values together.
result = a + b; // Add 'a' and 'b' and store the result in 'result'. 
  • - (Subtraction): Subtracts the second value from the first.
Copy Code
result = a - b; // Subtract 'b' from 'a' and store the result in 'result'.‎
 
  • * (Multiplication): Multiplies two values.
Copy Code
result = a * b; // Multiply 'a' by 'b' and store the result in 'result'.‎
 
  • / (Division): Divides the first value by the second.
Copy Code
result = a / b; // Divide 'a' by 'b' and store the result in 'result'.‎
 
  • % (Modulus): Computes the remainder of the division.
Copy Code
result = a % b; // Calculate the remainder when 'a' is divided by 'b' and ‎store it in 'result'.‎
 

2. Relational Operators:

  • == (Equal to): Checks if two values are equal.
Copy Code
equal = (a == b); // Set 'equal' to 1 if 'a' is equal to 'b', 0 otherwise.‎
 
  • != (Not equal to): Checks if two values are not equal.
Copy Code
not_equal = (a != b); // Set 'not_equal' to 1 if 'a' is not equal to 'b', 0 ‎otherwise.‎
 
  • < (Less than): Checks if the first value is less than the second.
Copy Code
less_than = (a < b); // Set 'less_than' to 1 if 'a' is less than 'b', 0 ‎otherwise.‎
 
  • > (Greater than): Checks if the first value is greater than the second.
Copy Code
greater_than = (a > b); // Set 'greater_than' to 1 if 'a' is greater than 'b', ‎‎0 otherwise.‎
 
  • <= (Less than or equal to): Checks if the first value is less than or equal to the second.
Copy Code
less_than_or_equal = (a <= b); // Set 'less_than_or_equal' to 1 if 'a' is less ‎than or equal to 'b', 0 otherwise.‎
 
  • >= (Greater than or equal to): Checks if the first value is greater than or equal to the second.
Copy Code
greater_than_or_equal = (a >= b); // Set 'greater_than_or_equal' to 1 if 'a' ‎is greater than or equal to 'b', 0 otherwise.‎
 

3. Logical Operators:

  • && (Logical AND): Performs a logical AND operation on two conditions.
Copy Code
result = (condition1 && condition2); // Set 'result' to 1 if both 'condition1' ‎and 'condition2' are true, 0 otherwise.‎
 
  • || (Logical OR): Performs a logical OR operation on two conditions.
Copy Code
result = (condition1 || condition2); // Set 'result' to 1 if either ‎‎'condition1' or 'condition2' is true, 0 otherwise.‎
 
  • ! (Logical NOT): Negates a logical condition.
Copy Code
result = !condition; // Set 'result' to the opposite of 'condition' (1 if ‎‎'condition' is false, 0 if 'condition' is true).‎
 

4. Bitwise Operators:

  • & (Bitwise AND): Performs a bitwise AND operation on two values.
Copy Code
result = a & b; // Perform a bitwise AND between 'a' and 'b' and store the ‎result in 'result'.‎
 
  • | (Bitwise OR): Performs a bitwise OR operation on two values.
Copy Code
result = a | b; // Perform a bitwise OR between 'a' and 'b' and store the ‎result in 'result'.‎
 
  • ^ (Bitwise XOR): Performs a bitwise XOR (exclusive OR) operation on two values.
Copy Code
result = a ^ b; // Perform a bitwise XOR between 'a' and 'b' and store the ‎result in 'result'.‎
 
  • ~ (Bitwise NOT): Performs a bitwise NOT (inversion) operation on a value.
Copy Code
result = ~a; // Invert all bits of 'a' and store the result in 'result'.‎
 
  • << (Bitwise Left Shift): Shifts bits to the left by a specified number.
Copy Code
result = a << 2; // Left shift 'a' by 2 bits and store the result in 'result'.‎
 
  • >> (Bitwise Right Shift): Shifts bits to the right by a specified number.
Copy Code
result = a >> 3; // Right shift 'a' by 3 bits and store the result in ‎‎'result'.‎

5. Concatenation Operator:

  • {} (Concatenation): Combines multiple signals or values into a single signal.
Copy Code
concatenated_signal = {signal_a, signal_b}; // Concatenate 'signal_a' and ‎‎'signal_b' into 'concatenated_signal'.‎
 

6. Conditional Operator:

  • ? : (Conditional operator): Provides a conditional assignment based on a condition.
Copy Code
result = (condition) ? value_if_true : value_if_false; // If 'condition' is ‎true, set 'result' to 'value_if_true', otherwise set it to 'value_if_false'.‎
 

7. Reduction Operators:

  • & (Reduction AND): Reduces multiple bits to a single bit using logical AND.
Copy Code
result = &{a, b, c}; // Computes the AND of 'a', 'b', and 'c' and stores the ‎result in 'result'.‎
 
  • | (Reduction OR): Reduces multiple bits to a single bit using logical OR.
Copy Code
result = |{a, b, c}; // Computes the OR of 'a', 'b', and 'c' and stores the ‎result in 'result'.‎
 
  • ^ (Reduction XOR): Reduces multiple bits to a single bit using logical XOR.
Copy Code
result = ^{a, b, c}; // Computes the XOR of 'a', 'b', and 'c' and stores the ‎result in 'result'.‎
 

8. Assignment Operator:

  • = (Assignment): Assigns a value to a variable or signal.
Copy Code
variable = value; // Assign 'value' to 'variable'.‎

9. Replication Operator:

  • {N{value}} (Replication): Replicates a value ‘N’ time to create a larger vector.
Copy Code
replicated_value = {4{data}}; // Replicate 'data' four times to create ‎‎'replicated_value'.‎
 

10. Increment and Decrement Operators:

  • ++ (Increment): Adds 1 to the variable.
Copy Code
a++; // Increment 'a' by 1.‎
 
  • -- (Decrement): Subtracts 1 from the variable.
Copy Code
b--; // Decrement 'b' by 1.‎
 

11. Logical Implication Operator:

  • ==> (Logical Implication): Computes logical implication between two conditions.
 
Copy Code
result = (condition1 ==> condition2); // Set 'result' to 1 if 'condition1' ‎implies 'condition2', 0 otherwise.‎
 

12. Case Equality Operator:

  • === (Case Equality): Compares two values for equality, including "x" and "z" values.
Copy Code
equal = (a === b); // Set 'equal' to 1 if 'a' and 'b' are equal, including "x" ‎and "z" values, 0 otherwise.‎
 

13. Case Inequality Operator:

  • !== (Case Inequality): Compares two values for inequality, including "x" and "z" values.
Copy Code
not_equal = (a !== b); // Set 'not_equal' to 1 if 'a' and 'b' are not equal, ‎including "x" and "z" values, 0 otherwise.‎
 

14. Wildcard Equality Operator:

  • ==? (Wildcard Equality): Compares two values for equality, treating "x" and "z" as don't care.
Copy Code
equal = (a ==? b); // Set 'equal' to 1 if 'a' and 'b' are equal, treating "x" ‎and "z" as don't care, 0 otherwise.‎
 

In conclusion, Verilog operators are fundamental building blocks for creating hardware descriptions in digital design. They enable you to perform a wide range of operations on data, control logic, and signals within FPGA and ASIC designs. Understanding and effectively using Verilog operators is essential for designing and simulating digital circuits accurately and efficiently.

Key takeaways:

  • Arithmetic Operators: Perform mathematical calculations such as addition, subtraction, multiplication, division, and modulus.
  • Relational Operators: Compare values to determine equality, inequality, and relative magnitude.
  • Logical Operators: Manipulate and evaluate logical conditions using AND, OR, and NOT operations.
  • Bitwise Operators: Perform operations at the bit level, including AND, OR XOR, and bit shifting.
  • Concatenation Operator: Combine multiple signals or values into a single signal.
  • Conditional Operator: Provide conditional assignments based on a specified condition.
  • Reduction Operators: Reduce multiple bits to a single bit using AND, OR, or XOR operations.
  • Assignment Operator: Assign values to variables or signals.
  • Replication Operator: Replicate values to create larger vectors.
  • Increment and Decrement Operators: Add or subtract from variables.
  • Logical Implication Operator: Evaluate logical implication between conditions.
  • Case Equality and Inequality Operators: Compare values for equality and inequality, including "x" and "z" values.
  • Wildcard Equality Operator: Compare values for equality, treating "x" and "z" as don't care.

These operators provide the flexibility to model a wide range of digital logic and control structures, allowing hardware designers to create complex and efficient digital systems. Whether you're designing simple combinational logic or intricate state machines, Verilog operators are indispensable tools for achieving your hardware design goals.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.