Maker.io main logo

How to Use MCP4725 12 Bit Digital to Analog Converter Using Arduino

11

2026-06-10 | By Ron Cutts

License: GNU Lesser General Public License I2C / TWI Microcontrollers PWM Arduino ESP32

In this tutorial, we will learn how to use the MCP4725 12-bit digital-to-analog converter with Arduino and Visuino to generate square, sine, and triangle waves.

Watch the video!

What You Will Need

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

What You Will Need photo 7

What You Will Need photo 8

The Circuit

  • Connect Arduino pin [5V] to breadboard positive pin [Red line]

  • Connect Arduino pin [GND] to breadboard negative pin [Black line]

  • Connect MCP4725 pin [Out] to 1K ohm Resistor on the breadboard

  • Connect other side of the Resistor to the LED pin [positive +]

  • Connect LED pin [negative - ] to the breadboard negative pin [Black line]

  • Connect MCP4725  pin [SCL] to Arduino pin [SCL]

  • Connect MCP4725 pin [SDA] to Arduino pin [SDA]

  • Connect MCP4725  pin [VCC] to breadboard positive pin [Red line]

  • Connect MCP4725   pin [GND] to breadboard positive pin [Black line]

  • Connect Oscilloscope Signal probe to MCP4725 pin [Out]

  • Connect Oscilloscope Ground probe to breadboard positive pin [Black line]

The Circuit

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type photo 2

Generate Square Waves - in Visuino Add & Set Components

  • Add "Microchip I2C Digital To Analog Converter (DAC) - MCP4725" component

  • Add "Square Analog Generator" component

  • Connect "SquareAnalogGenerator1" pin [Out] to "DAC1" pin [In]

  • Connect "DAC1" pin I2C [Out] to the Arduino Board pin I2C [In]

  • Upload the Project to the board; see the "Generate, Compile, and Upload the Arduino Code" Step on how to upload the project

Generate Square Waves - in Visuino Add & Set Components

Generate Square Waves - in Visuino Add & Set Components photo 2

Generate Square Waves - in Visuino Add & Set Components photo 3

Generate Sine Waves - in Visuino Add & Set Components

  • Add "Microchip I2C Digital To Analog Converter (DAC) - MCP4725" component

  • Add "Sine Analog Generator" component

  • Set the "Frequency" in the Properties window to 0.2

  • Connect "SineAnalogGenerator1" pin [Out] to "DAC1" pin [In]

  • Connect "DAC1" pin I2C [Out] to the Arduino Board pin I2C [In]

  • Upload the Project to the board; see the "Generate, Compile, and Upload the Arduino Code" Step on how to upload the project

Generate Sine Waves - in Visuino Add & Set Components

Generate Sine Waves - in Visuino Add & Set Components photo 2

Generate Sine Waves - in Visuino Add & Set Components photo 3

Generate Sine Waves - in Visuino Add & Set Components photo 4

Generate Triangle Waves - in Visuino Add & Set Components

  • Add "Microchip I2C Digital To Analog Converter (DAC) - MCP4725" component

  • Add "Triangle Analog Generator" component

  • [Optional] Set the "Frequency" in the Properties window

  • Connect "TriangleAnalogGenerator1" pin [Out] to "DAC1" pin [In]

  • Connect "DAC1" pin I2C [Out] to the Arduino Board pin I2C [In]

  • Upload the Project to the board; see the "Generate, Compile, and Upload the Arduino Code" Step on how to upload the project

Generate Triangle Waves - in Visuino Add & Set Components

Generate Triangle Waves - in Visuino Add & Set Components photo 2

Generate Triangle Waves - in Visuino Add & Set Components photo 3

Generate Digital Pulses - in Visuino Add & Set Components

  • In this Example we are going to convert digital pulses from "Pulse Generator" component to an analog signal using a "Digital To Analog" component

  • Add "Microchip I2C Digital To Analog Converter (DAC) - MCP4725" component

  • Add "Pulse Generator" component

  • [Optional] Set the "Frequency" in the Properties window

  • Add "Digital To Analog" component

  • [Optional] Set the "True" or "False" values in the Properties window

  • Connect "PulseGenerator1" pin [Out] to "DigitalToAnalog1" pin [In]

  • Connect "DigitalToAnalog1" pin [Out] to "DAC1" pin [In]

  • Connect "DAC1" pin I2C [Out] to the Arduino Board pin I2C [In]

  • Upload the Project to the board; see the "Generate, Compile, and Upload the Arduino Code" Step on how to upload the project

Generate Digital Pulses - in Visuino Add & Set Components

Generate Digital Pulses - in Visuino Add & Set Components photo 2

Generate Digital Pulses - in Visuino Add & Set Components photo 3

Generate Digital Pulses - in Visuino Add & Set Components photo 4

Generate Digital Pulses - in Visuino Add & Set Components photo 5

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, and then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

If you power the board, the LED will blink, and if you are using an oscilloscope, you should see the signal from the MCP4725 module. There are many ways to use this module; this was just a quick simple introduction to get started.

Note: In my project, I set the I2C address of the "Microchip I2C Digital To Analog Converter (DAC) - MCP4725" to 96, you should check the address of your module.

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this. You can download it here and open it in Visuino: https://www.visuino.eu

Downloads

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.